SNAA421 November 2025 LMK05318B , LMK5B12204 , LMK5B33216 , LMK5B33414 , LMK5C33216A , LMK5C33414A
The APLL cannot lock without a valid APLL reference and the DPLL cannot lock without a locked APLL. Therefore, the best practice is to check the APLL reference input clock. The APLL reference is commonly sourced from an external XO, TCXO, or OCXO. However, the LMK device also supports casaded APLL operation, using one APLL output as the APLL reference of another APLL. Figure 2-1 provides an example cascaded scheme. APLLx is the upstream APLL (cascaded source) and the APLL reference is the XO input. APLLy is the downstream APLL (cascaded APLL) and the APLL reference is the cascaded source.
Throughout the application note, the term "XO input" refers to any external source used as the APLL reference and the term "cascaded source" refers to any internal APLL source used as the APLL reference.
Proceed to Is the APLL Locked? if the APLL reference is considered valid but the APLL and DPLL are not locked. Otherwise, refer to Check Status of APLL Reference and Debug APLL Reference.