SPRACY5 July   2021 AM67 , AM67 , AM67A , AM67A , AM68 , AM68 , AM68A , AM68A , AM69 , AM69 , AM69A , AM69A , DRA821U , DRA821U , DRA821U-Q1 , DRA821U-Q1 , DRA829J , DRA829J , DRA829J-Q1 , DRA829J-Q1 , DRA829V , DRA829V , DRA829V-Q1 , DRA829V-Q1 , TDA4AEN-Q1 , TDA4AEN-Q1 , TDA4AH-Q1 , TDA4AH-Q1 , TDA4AL-Q1 , TDA4AL-Q1 , TDA4AP-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4APE-Q1 , TDA4VE-Q1 , TDA4VE-Q1 , TDA4VEN-Q1 , TDA4VEN-Q1 , TDA4VH-Q1 , TDA4VH-Q1 , TDA4VL-Q1 , TDA4VL-Q1 , TDA4VM , TDA4VM , TDA4VM-Q1 , TDA4VM-Q1 , TDA4VP-Q1 , TDA4VP-Q1 , TDA4VPE-Q1 , TDA4VPE-Q1

 

  1.   Trademarks
  2. 1Introduction to Flashing Tools
    1. 1.1 Trace32/Lauterbach
    2. 1.2 CCS-Based Flash Writer
    3. 1.3 Other Software Tools
  3. 2Flash Devices on TDA4
    1. 2.1 Flashing OSPI and eMMC RAW Sectors
    2. 2.2 Flashing eMMC User Partition
  4. 3Prerequisites for Flashing TDA4
    1. 3.1 Boot Switch Settings
    2. 3.2 How to Generate a Tiny File System
    3. 3.3 Generating the eMMC tisdk-tiny-image.img
    4. 3.4 Running Until u-boot
      1. 3.4.1 UART Boot Mode
      2. 3.4.2 DFU Boot
      3. 3.4.3 SD Boot or any Other Boot Mode
    5. 3.5 Configuring Boot0 Partition and Partitioning eMMC
  5. 4OSPI Flashing
    1. 4.1 Flashing Bootloader Binaries
      1. 4.1.1 TI UNIFLASH Tool
        1. 4.1.1.1 Flashing Instructions
        2. 4.1.1.2 Linux Boot Binaries
        3. 4.1.1.3 RTOS Boot Binaries
    2. 4.2 dfu-util
      1. 4.2.1 Flashing Instructions
    3. 4.3 CCS/JTAG
      1. 4.3.1 Flashing Instructions
    4. 4.4 Trace32/Lauterbach
      1. 4.4.1 Flashing Instructions
    5. 4.5 u-boot
      1. 4.5.1 Flashing Instructions
  6. 5eMMC flashing
    1. 5.1 Flashing Bootloader Binaries
      1. 5.1.1 TI UNIFLASH Tool
        1. 5.1.1.1 Flashing Instructions
      2. 5.1.2 Trace32/Lauterbach
        1. 5.1.2.1 Flashing Instructions
      3. 5.1.3 dfu-util
        1. 5.1.3.1 Flashing Instructions
    2. 5.2 u-boot
      1. 5.2.1 Flashing Instructions
    3. 5.3 eMMC UDA Partition Flashing With tinyrootfs
      1. 5.3.1 dfu-util
      2. 5.3.2 u-boot + CCS/JTAG
        1. 5.3.2.1 Flashing Instructions

Flashing Instructions

  1. Halt at u-boot.
  2. Connect CCS using the XDS110/XDS560v2 and using the appropriate target ccxml (without GEL files).
  3. Load the tisdk-tiny-image.img to the DDR address 0x80080000. In this document, see Section 3.2 for the tiny file system and then Section 3.3 to create the *.img.
    1. Launch the target ccxml and connect to CortexA72_0_0.
    2. Open Memory browser and load memory: View -> Memory Browser -> Load Memory.
    3. Select file tisdk-tiny-image.img and select File Type as Binary, click Next.
    4. Set Start Address as 0x80080000, click Finish.
    5. Depending on the JTAG used, the time taken to load this will vary. Expect 1 hour with XDS110 and 20 minutes with XDS560v2.
  4. The image is loaded on the RAM, flash it using u-boot.
    # Run the below command from u-boot prompt
    => part start mmc 0 rootfs
             
    # what ever the above command outputs, use that below (eg - 0x22)
    => mmc write 0x80080000 0x22 0x32000
     
    # after the above completes
    => boot