Pattern On-The-Fly Mode is the
easiest and quickest way to create a pattern sequence. Follow these steps to create
a simple pattern sequence using three images
- Make sure the EVM is powered up and operating correctly, and
the Connected radio-button is lit green.
- Select Pattern On-The-Fly Mode from the Operating
Mode group box, and then click the Pattern Design button so that
the large black panel is displayed as shown in Figure 4-6.
- Click the Add Pattern button in the Menu bar and
browse for any three bitmap images from the sample of images directory. Be sure
to select them from the correct image folder for the EVM that is being used. All
three images can be selected at the same time within the open file dialog
window. When selecting multiple files at once, the operating system may not load
the images in the same order as they were selected. To add images in a
predefined order, use the Load button. This option loads the images from
a text file that contains the file names of each bitmap in the desired order.
Alternatively, you can add the images one at a time using the Add Pattern
button to ensure order. Figure 4-8 shows an example of loading images from a file. The bitmap images must be
located in the same directory as the text file. See Figure 4-9 after the images have been added.
- Each pattern in the display can now be
selected individually or a multiple selection can be done. To select multiple
patterns in a series, use Shift+Click. To select multiple patterns that
are not in a series, use Ctrl+Click. An alternate method for selecting
all images is to use the Select All Patterns button on the Menu
bar.
- Select the first pattern and choose a bit depth of 1. Set
exposure to 100000 µs and set dark time to 50000 µs. The dark time is the time
from the end of one pattern to the start of the next pattern. Select Red for the color.
- Select the second pattern and choose a bit depth of 1. Set
exposure to 150000 µs and set dark time to 75000 µs, and select Green as the color.
- Select the third pattern and choose a bit depth of 1. Set
exposure to 200000 µs and set dark time to 100000 µs, and select Blue as the color. Figure 4-10 shows the pattern sequence. The Zoom bar can be used to zoom in and
out which is useful when many patterns are loaded into the panel.
- Select the Repeat radio-button to continuously repeat the
pattern sequence, or, if only one time is desired, then select the Play
Once radio-button.
- Click the Update LUT button to upload the pattern
sequence definition, including the three pattern images, to the DLPC900. Notice
the green status bar indicating that the updated LUT is uploading to the EVM.
This animation does not occur if the user only edits pattern settings rather
than uploading actual new patterns. If there are any errors in the pattern
sequence, the GUI displays an error message.
- Once the upload is complete, click the Start button. The
display repeatedly displays the Red, Green, and Blue dots.
- To pause the pattern sequence, click the Pause button.
To continue from where the pattern sequence paused, click the Start
button.
- To stop the pattern sequence, click the Stop button. To
restart the pattern sequence click the Start button. The pattern sequence
starts from the beginning whenever the pattern sequence is stopped using the
Stop button.
Another method of creating a pattern
sequence in Patten On-The-Fly Mode is using a batch file that contains all
the necessary commands and the compressed images.
Follow these steps to execute a
pattern sequence using a batch file.
- Stop the pattern sequence if it is currently running.
- Click the Batch Files button at the top of the GUI.
- Check the box to Enable Command Logging.
- Click the Clear All button to clear any content in the
panel.
- Click the Load Batch File button and select the
onthefly.txt file located in the sample images directory. Be sure to
select the correct file for the EVM being used.
- Click the Execute All button. Wait for the batch file to
execute.
- Click the Pattern Mode button at the top of the
GUI.
- Click the Start button.
- Click the Stop button to end this example.