DLPU102B December 2020 – July 2022
Creating a Pre-Stored Pattern sequence is very similar to Pattern On-The-Fly Mode. The difference is that the patterns are pre-stored in flash memory.
If images are not present in the flash memory, proceed to Section 4.9.1 section to add the images to the firmware and upload them to the EVM, then return here for steps on creating the pattern sequence.
To start creating a Pre-Stored Pattern sequence, follow the steps in Section 4.6.2 with the only change in step 2. In step 2, select the Pre-Stored Patten radio-button and then proceed with step 3.