SLASFL3 September 2026 DAC90802
PRODUCTION DATA
At high output voltage swings (>15VPP) and high output frequencies, the third harmonic distortion (HD3) of the DAC90802 can be sub-optimal. To mitigate this, the DAC90802 provides a correction mechanism through the CHx_CFG registers By adjusting the 9-bit VREF_SQx field (values ranging from 0 to 511), users can optimize harmonic performance.
The recommended value for VREF_SQx is calculated using the following equation:
where
Figure 8-5 illustrates the relationship between the normalized vref sq value and frequency (kHz). The normalized vref sq value is defined by the following relationship:
Figure 8-5 Optimised Normalized Vref Sq
Value vs Frequency(kHz)