SLUUDB4 June 2025 TAS5830
The input mixer can be used to mix the left and right channel input signals as shown in Figure 3-1. The input mixer has four coefficients, which control the mixing and gains of the input signals.
Figure 3-1 Input MixerThe Basic Tab (See Figure 3-2) provides the easiest way for configuration in PPC3 GUI. Switch to the Advanced tab (See Figure 3-3) to adjust all the four coefficients manually. Note that the four parameters need to be specified in decibels (dB). You can invert the result of any of the gains by clicking on the "+" that is placed after the coefficient box in the GUI.
Figure 3-2 Input Mixer (Basic Tab)
Figure 3-3 Input Mixer (Advanced Tab)