SPRABV4I October   2021  – August 2025 F28377D-SEP , SM320F28335-EP , SM320F28335-HT , TMS320F280023-Q1 , TMS320F280025-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Programming Fundamentals
  6. 3ROM Bootloader
  7. 4Flash Kernel A
    1. 4.1 Implementation
      1. 4.1.1 Application Load
  8. 5Flash Kernel B
    1. 5.1 Implementation
      1. 5.1.1 Packet Format
      2. 5.1.2 CPU1 Kernel Commands
      3. 5.1.3 CPU2 Kernel Commands
      4. 5.1.4 Packet Data
      5. 5.1.5 Status Codes
    2. 5.2 F2838x SCI Flash Kernels
      1. 5.2.1 CPU1-CPU2 Kernels
        1. 5.2.1.1 Kernel Commands
      2. 5.2.2 CPU1-CM Kernels
        1. 5.2.2.1 Kernel Commands
      3. 5.2.3 Using the Projects With SCI Bootloader
        1. 5.2.3.1 CPU1-CPU2
        2. 5.2.3.2 CPU1-CM
      4. 5.2.4 Using the Projects With Code Composer Studio (CCS) Software
        1. 5.2.4.1 CPU1-CPU2
        2. 5.2.4.2 CPU1-CM
    3. 5.3 F28P65x SCI Flash Kernel
      1. 5.3.1 CPU1 Kernel
        1. 5.3.1.1 Host-Kernel Communication: ControlCard
        2. 5.3.1.2 Host-Kernel Communication: LaunchPad Development Kit
        3. 5.3.1.3 Kernel Commands
      2. 5.3.2 Using the Projects With SCI Bootloader
        1. 5.3.2.1 CPU1
      3. 5.3.3 Using the Projects With CCS
        1. 5.3.3.1 CPU1
    4. 5.4 F28P55x SCI Flash Kernel
      1. 5.4.1 Implementation
        1. 5.4.1.1 Specifying the Flash Banks and Sectors of the Application
      2. 5.4.2 Kernel
      3. 5.4.3 Using the Project With SCI Bootloader
      4. 5.4.4 Using the Project with CCS
  9. 6Example Implementation
    1. 6.1 Device Setup
      1. 6.1.1 Flash Kernels
      2. 6.1.2 Hardware
    2. 6.2 Host Application: serial_flash_programmer
      1. 6.2.1 Overview
      2. 6.2.2 Building and Running serial_flash_programmer Using Visual Studio
      3. 6.2.3 Running serial_flash_programmer for F2806x (Flash Kernel A)
      4. 6.2.4 Running serial_flash_programmer for F2837xD (Flash Kernel B)
    3. 6.3 Host Application: Firmware Updates on F28004x With SCI Flash Kernel
      1. 6.3.1 Overview
      2. 6.3.2 Boot Pin Configurations
      3. 6.3.3 Using Three Boot Modes
      4. 6.3.4 Performing Live Firmware Updates
  10. 7Troubleshooting
    1. 7.1 General
    2. 7.2 SCI Boot
    3. 7.3 F2837x
      1. 7.3.1 F2837xS
      2. 7.3.2 F2837xD
      3. 7.3.3 F2837xD LaunchPad™
    4. 7.4 F28P65x
  11. 8References
  12. 9Revision History

F2837xD

Question: I want to boot from Flash and SCI, how do I switch between the two? Flash Boot is used for normal operation, SCI Boot for firmware update.

Answer:

There are a few options here. A few are mentioned in Section 6.3 - the device can boot up in Flash boot mode for normal operation, and in SCI Boot mode for firmware upgrades. The user needs to design a scheme that allows changing the boot mode select pins settings. Alternately, the user can decide to only use the Flash boot mode, and then in software, branch to the SCI Boot function. This can be through an IO trigger or host command, that serves as a cue to call the SCI_Boot() function. The advantage of this approach is that the user does not need to change the boot mode select pins settings. Note that in this case, the SCI ROM Bootloader is not invoked.

Question: Using SCI Boot mode to upgrade firmware works, however using Flash boot and branching to SCI Boot in software by calling SCI_Boot() does not work. What must I look at to fix this?

Answer:

  • Make sure the correct GPIO pins are being used for SCI boot mode.
  • Also,disabling the watchdog and interrupts prior to the SCI_Boot() call in your program is necessary, since Flash is being updated.

Question: With the ControlCARD, I cannot download the SCI Flash Kernel to RAM in SCI Boot, what steps must I take to do so?

Answer:

  1. The controlCARD requires that option 2 of SCI Boot be used for the controlCARD to work on the device. For more details, see the Warnings/Notes/Errata section of [12]. To do this, make sure the SCI Flash Kernel project builds with SCI_BOOT_ALTERNATE as the parameter for SCI_GetFunction.
  2. Next, set the SW1:A position 1 to ON on the controlCARD. This allows the emulator to be connected. Set the Boot mode to SCI by setting SW1 Position 1 to 0, and SW1 Position 2 to 1.
  3. After that, make sure that SW1:A position 2 is also ON. GPIO28 (and pin 76 of the 180-pin controlCARD connector) is coupled to the FTDI’s USB-to-Serial adapter. This allows UART communication to a computer through the FTDI chip.
  4. After this, connect the emulator via CCS. Launch the target configuration file for the controlCard and connect to CPU1. Open up a Memory Window (View > Memory Window) and look up the location 0xD00 in memory. Change 0xD00 to 0x815A. To use Alternate GPIOs (28, 29) for SCI Boot mode, we need to set the BMODE field (bits 15:8) of the corresponding BOOTCTRL register (either EMUBOOTCTRL (0xD00) or Z1-BOOTCTRL (0x7801E which is in User configurable DCSM OTP) to 0x81).
  5. If you wish to run the flash kernel on CPU2 as well, connect to the flash kernel in CCS. Click "Reset CPU", followed by "Resume". The program hits ESTOP. Click "Resume" again.
  6. In CCS, for CPU1, click "Reset CPU", followed by "Resume" (F8).
  7. Now, run the command serial_flash_programmer.exe with the appropriate command. The kernel is downloaded to RAM. When the menu pops up, select the desired operation to proceed. To see what the command window looks like at this stage, see Figure 6-1.