SPRAD06C March 2022 – March 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62L
The region of the PCB used for DDR4 circuitry must be isolated from other signals. The DDR4 keepout region is defined for this purpose and is shown in Figure 2-4. The size of this region varies with the placement and DDR routing. Non-DDR4 signals must not be routed on the DDR signal layers within the DDR4 keepout region. Non-DDR4 signals can be routed in this region only if the signals are routed on other layers separated from the DDR signal layers by a ground layer. No breaks are allowed in the reference ground layers in this region. In addition, a solid VDDS_DDR power plane exists across the entire keepout region.