The DDR4 interface schematics vary,
depending upon the width of the DDR4 SDRAM devices used and the width of the EMIF bus
implemented. General connectivity is straightforward and consistent between the
implementations. 16-bit SDRAM devices look like two 8-bit devices. Figure 2-1 shows the schematic connections for a 16-bit interface using a single x16 SDRAM.
- When designing with VTT regulator (LDO),
which can source and sink current, decoupling capacitors (minimum of one capacitor (1.0uF
value) must be used for every two termination resistors) must be used to minimize the
effect of VTT supply noise. Refer to the AM64x GP EVM for
reference
- Zo value for resistors is 30-47ohm.
Resistor value must closely match trace impedance.
- VTT is optional on address and control
signals when using single package memory devices, but termination as shown on CK0/CK0_n is
always required
- DDR_VREF is supplied by the VTT
regulator. When VTT is not used, VREFCA needs to be connected to a voltage divider.
Consult the EVM schematic for an example of the voltage divider implementation.
- An external 240Ω ±1% resistor must be
connected between the DDR0_CAL0 pin and VSS. The maximum power dissipation for the
resistor is 5.2mW. No external voltage must be applied to the DDR0_CAL0 pin. Tolerance of
±1% required throughout life of component or product.
- RESET_n shall have an external 10k
pull-down resistor to control RESET low until the DDR controller drives the signal.
RESET_n has no length matching requirement.