LPDDR4 supports many different
implementation topologies. However, the devices only support a single 16-bit channel
for LPDDR4. SDRAMs with additional channels and/or dies can be implemented but the
additional channels or dies are unconnected and not used. Table 3-1 lists the only supported LPDDR4 device combination.
Table 3-1 Supported LPDDR4 SDRAM
Combinations
| LPDDR4 SDRAM Count |
Channels |
Die |
Ranks(CS signals) |
LPDDR4 Channel Width |
DDRSS data width |
Schematic |
Max Addressable Range |
| 1 |
1 |
1 |
1(CS0_n) |
16 |
16 |
Figure 3-1 |
2GBytes |
Note: ECC is supported on the LPDDR4 interface. Unlike
traditional ECC interfaces, which require dedicated memory pins and devices, ECC is
supported inline. The ECC system impact is in interface bandwidth and overall memory
density, as ECC data is stored alongside non-ECC data. Max addressable range is
reduced if ECC is enabled. See device TRM for more details.
Note: Data bus routing must be point to
point between the processor and the memory, and cannot be split on the board. Thus,
dual-rank LPDDR4 designs are only possible when using one channel of an LPDDR4 dual
channel, dual rank device. If more than 2GBytes is needed, consider using
DDR4.