SPRAD06C March 2022 – March 2025 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62L
Figure 2-3 shows the required placement for the processor and the DDR4 devices. The dimensions for this figure are defined in Table 2-3. The placement does not restrict the side of the PCB on which the devices are mounted. The ultimate purpose of the placement is to limit the maximum trace lengths and allow for proper routing space.
| Number | Parameter | MIN | MAX | UNIT |
|---|---|---|---|---|
| 1 | x1 | 2000 | Mils | |
| 2 | y1 | 500 | Mils | |
| 3 | y2 | 1000 | Mils | |
| 4 | y3 | 750 | Mils |