SPRADP6A February 2025 – May 2025 AM2612 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
After connecting the AM26x UART0 interface to the host PC, open the Device Manager or similar application to verify that the UART ports are being detected.
Figure 4-1 AM26x UART Port DetectionOnce verified, open a UART terminal application, such as Tera Term.
In the Tera Term window, select Setup → Serial Port, and configure the following settings:
Click New Open. Assert the AM26x Power-On-Reset (PORz), which is accomplished by triggering a PORz reset circuit on the PCB, or by simply power cycling the PCB system.
Figure 4-2 Tera Term SetupAfter power cycling the AM26x, the ASCII character 'C' prints to the UART console. This confirms that the AM26x is alive and is booting via UART.
Figure 4-3 AM26x UART Boot Console OutputIf Cs are not printing to the UART console, then make sure the following are checked.
Figure 4-4 UART Console After Power-on-Reset,
with Cs Printing At the End of the UART Output