SPRADP6A February   2025  – May 2025 AM2612 , AM2612-Q1 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Power Net Checks
    1. 2.1 Verify Proper AM26x Power Rail Voltage Levels
    2. 2.2 Verify Maximum Current Loading
    3. 2.3 AM26x Power Sequencing
    4. 2.4 AM26x Power Topology References
  6. 3Device Boot Status
    1. 3.1 AM26x SOP Pin Status
    2. 3.2 SOP Boot Mode Latch Timing
    3. 3.3 AM26x SOP Pin Isolation
  7. 4Verify UART Output
    1. 4.1 Configure AM26x for UART Boot
    2. 4.2 Configure Host PC for UART Boot Validation
  8. 5Verify JTAG Connection
    1. 5.1 Configure AM26x for JTAG
    2. 5.2 Configure Host PC for JTAG Debug
    3. 5.3 Test the JTAG Connection
    4. 5.4 Connect to the AM26x R5F Core
  9. 6Loading and Executing a Code Example
    1. 6.1 Importing, Building, and Loading the Project
  10. 7Summary
  11. 8References
  12. 9Revision History

Importing, Building, and Loading the Project

Note: Make sure that the latest AM26x MCU+ Software Development Kit is installed on the host PC.

Import the Project

  1. In Code Composer Studio, select File → Import.
     Import Project Figure 6-1 Import Project
  2. Select CCS Projects.
  3. In the Import window, select Browse and navigate to mcu_plus_sdk_{AM26x_device_name}_{version}\examples\hello_world\am263px-cc\r5fss0-0_freertos\ti-arm-clang.
  4. Click Finish.

Build the Project

In the Project Explorer window, right-click the project name and select Build Project.

 Build Project Figure 6-2 Build Project

After the project has completed building, connect to the R5_0 core of the target connection as outlined in Section 5.4 if this is not done already.

Load the Program

  1. In the CCS toolbar, click Run → Load → Load Program.
     Load Program Figure 6-3 Load Program
  2. In the Load Program window, select Browse Project and navigate to the Release folder of the CCS project.
     Release Folder Figure 6-4 Release Folder
  3. Click OK to load the project binary file to the AM26x device R5_0 Core.
    Note: If the program load fails, then perform a CPU reset by selecting the CPU Reset icon in the CCS toolbar. Then re-load the program.
     CPU Reset Figure 6-5 CPU Reset
  4. Click the Play (Resume) button in the CCS toolbar to run the binary on the AM26x device.
     Resume Binary Figure 6-6 Resume Binary
  5. Observe the console output. The proper output is in Figure 6-7.
     Hello World Console Output Figure 6-7 Hello World Console Output

The basic checks for bringing up a custom PCB with an AM26x device are now complete.