SPRADP6A February 2025 – May 2025 AM2612 , AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
To check the AM26x UART output, the device must first be placed into UART boot mode.
If the PCB design accounts for a configurable boot mode (that is, through DIP switches), then set the SOP[3:0] switches to 0001. This SOP[3:0] setting for UART boot mode applies for all AM26x devices.
If the PCB design has a fixed boot mode configured by soldered pull resistors, then this is likely that the AM26x is set in a boot mode with UART Fallback. To confirm, see Section 3.1.
Once UART boot mode is set, connect the AM26x PCB system to a host PC using any USB to UART adapter. Make sure that the UART0 instance TX, RX pins are being used to connect to the host PC. TI recommends the XDS110 JTAG Debug Probe, which is supported for use by all AM26x microcontrollers, and is well integrated with the TI software and debug tools.