SPRADR6 April   2025 F28377D-SEP , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Getting Started
  5. 2Overview
  6. 3Migration Support Feature
    1. 3.1 Project Detection
    2. 3.2 Setup Migration Settings Page
    3. 3.3 Migration Execution
      1. 3.3.1 Running Migration Check on a Standalone File
      2. 3.3.2 Running Migration Check on a Project
    4. 3.4 Quick Fixes
    5. 3.5 Migration Report
    6. 3.6 Bitfield Migration
  7. 4Summary
  8. 5References

Migration Support Feature

The C2000 IDEA tool simplifies code migration between C2000 devices by automatically identifying and highlighting changes in driverlib code, including added, removed, or modified Application Peripheral Interfaces (APIs), registers, fields, enums, and macros. This automation reduces manual effort, minimizes the risk of errors, and verifies a smooth and efficient migration process. The automation supports migration for both complete projects and standalone driverlib files, providing flexibility to meet various user requirements. For specific devices, the tool also enables bitfield code migration. C2000 IDEA simplifies migration between F28x-to-F28x and F28x-to-F29x devices by detecting architectural differences and offering targeted recommendations for a more reliable transition. Table 3-1 provides a clear summary of migration support across C2000 devices, helping users quickly assess compatibility and available support for both Driverlib and Bitfield implementations.

Table 3-1 Migration Support for C2000 Devices

Device Families

Driverlib Migration Support

Bitfield Migration Support

F29H85x

Yes

No

F28P55x

Yes

No

F28P65x

Yes

No

F28002x

Yes

No

F28004x

Yes

No

F28003x

Yes

No

F280013x

Yes

Yes (To)

F280015x

Yes

No

F2838x

Yes

No

F2837x

Yes

No

F2807x

Yes

No

F2803x

No

Yes(From)

This tool supports source files in specific file formats, as illustrated in Table 3-2.

Table 3-2 Migration Support for Various File Formats

Source File Format

Migration Support

*.c

Yes

*.h

Yes

*.asm

No

*.cmd

No

*.lib

No

Linker Files

No

Figure 3-1 outlines the key steps required to migrate a standalone file or an entire project, to make sure of a seamless and efficient migration process

 C2000 IDEA - Migration Flow Figure 3-1 C2000 IDEA - Migration Flow