SPRSP91C February 2023 – November 2025 AM68 , AM68A
PRODUCTION DATA
Figure 6-29 shows the recommended oscillator connections when OSC1 is connected to a 1.8-V LVCMOS square-wave digital clock source.
A DC steady-state condition is not allowed on OSC1_XI when the oscillator is powered up. This is not allowed because OSC1_XI is internally AC coupled to a comparator that may enter a unknown state when DC is applied to the input. Therefore, application software should power down OSC1 any time OSC1_XI is not toggling between logic states.
Figure 6-34 1.8-V LVCMOS-Compatible Clock Input