SPRT759A October 2023 – June 2024 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
| Terminology and Abbreviations | Definition |
|---|---|
| A.x... | Reference from the UL 1998 standard. For example: A.7.1.19 is a specific definition found in appendix A of the standard. |
| C28x | A C2000 central processing unit. |
| CLA | C2000 Control Law Accelerator: an independent 32-bit floating-point processor. |
| CLA PROM | Program ROM for the CLA CPU |
| CLB | C2000 Configurable Logic Block |
| Class B / 1 | IEC 60730 Class B and UL 1998 Class 1. Class assigned based on a functional safety assessment. Refer to c. |
| Class C / 2 | IEC 60730 Class C and UL 1998 Class 2: Class assigned based on a functional safety assessment. Refer to Table 1. |
| CLK | Clock |
| CPU | Central Processing Unit |
| CPU Timer | C2000 general timer peripheral |
| CRC | Cyclic Redundancy Check |
| DC fault | (IEC/UL) Short circuits between signals. |
| DCC | C2000 dual clock comparitors |
| DCSM | C2000 dual code-security module |
| ECC | Error correction code |
| E/E/PE | (IEC/UL) Electrical/Electronic/Programmable Electronic |
| EMC | (IEC/UL) Electromagnetic compatibility |
| ePIE | C2000 enhanced peripheral interrupt expansion block. May also be referred to as PIE. |
| ePWM | C2000 enhanced Pulse Width Modulation peripheral. May also be referred to as PWM. |
| FPU | Floating-point Unit instruction set extension to the C28x CPU |
| FSM |
|
| GPIO | C2000 general purpose input/output pin |
| H.x... | Reference from the IEC 60730 standard. For example: H.2.16.5 is a specific definition found in annex H of the standard. |
| HRPWM | High-resolution feature of the C2000 ePWM module |
| HW | Hardware (the microcontroller) |
| HWBIST | C2000 hardware built-in self test |
| IEC | International Electrotechnical Commission |
| IEC 60730 | The terms "IEC 60730", "UL 1998", "IEC / UL standards", "60730" and
"the standards" are used interchangeably to refer to both:
|
| IEC 61508 | IEC 61508 Functional Safety of Electrical/Electronic/Programmable Electronic Safety-Related Systems, International Electrotechnical Commission, Edition 2.0 2010. |
| ISO 26262 | ISO 26262–Road Vehicles-Functional Safety, International Standard ISO, vol. 26262, 2018. |
| IEC / UL | Short for the standards or indicates something taken from the standards. Such as (IEC/UL) marked definitions in this list. See IEC 60730 |
| MPOST | Memory power-on self-test |
| PIE | See ePIE. |
| PWM | See ePWM. |
| PEST | Periodic self-test |
| POST | Power-on self-test |
| ROM | Read only memory |
| SDL | Software Diagnostic Library |
| SRAM | Static random-access memory |
| STL | Self-Test Library |
| Stuck-at | (IEC/UL) An open circuit fault or non-varying signal level |
| SW | Software |
| TI | Texas Instruments Inc. |
| TMU | Trigonometric Math Unit instruction set extension to the C28x CPU |
| UL | Underwriters Laboratories Inc. |
| UL 1998 | See IEC 60730 |
| Unique ID | A C2000 unique identifier assigned to a functional safety feature or diagnostic in the functional safety manual. For example CLK2 or GPIO4. |
| VCRC | Refer to VCU |
| VCU | Instruction set extension to the C28x CPU. Part of the added instructions are CRC calculation specific. The CRC instructions are supported on some devices as simply the "VCRC". |