SPRUHM8K December 2013 – May 2024 F28377D-SEP , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
Figure 21-19 and Figure 21-20 show the clock and frame-synchronization operation with various polarities of CLKR and FSR. These figures assume FWID = 0 in SRGR1, for an FSG pulse that is one CLKG cycle wide. The FPER bits of SRGR2 are not programmed; the period from the start of a frame-synchronization pulse to the start of the next pulse is determined by the arrival of the next inactive-to-active transition on the FSR pin. Each of the figures shows what happens to CLKG when it is initially synchronized and GSYNC = 1, and when it is not initially synchronized and GSYNC = 1. Figure 21-20 has a slower CLKG frequency (it has a larger divide-down value in the CLKGDV bits of SRGR1).
Figure 21-19 CLKG Synchronization and FSG Generation When GSYNC = 1 and CLKGDV = 1
Figure 21-20 CLKG Synchronization and FSG Generation When GSYNC = 1 and CLKGDV = 3