SPRUHM8K December 2013 – May 2024 F28377D-SEP , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
Table 4-52 details the NAK status information for CPU1, if boot ROM IPC command support is enabled. These NAK status bits are returned by CPU1 in the C2TOC1IPCDATAR[11:0] register.
| Bit | Description |
|---|---|
| 3-0 | 0 – Invalid Value or value isn’t set |
| 1 – Command not supported | |
| 2 – Command not set correctly | |
| 3 – CPU is trying to send a second command before the first one is complete | |
| 4 – Command execution resulted in an error | |
| 5 – Command cannot be executed in the current state of the boot ROM |