| ADC |
ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt
Mode) is not Set |
Yes |
Yes |
Yes |
| MCAN |
Message Order Inversion When Transmitting From Dedicated Tx
Buffers Configured With Same Message ID |
Yes |
Yes |
Yes |
| ePWM |
ePWM: An ePWM Glitch can Occur if a Trip Remains Active at the
End of the Blanking Window |
Yes |
Yes |
Yes |
| ePWM |
ePWM: ePWM TZFRC and TZCLR Events may be Missed When
PERCLKDIVSEL.EPWMCLKDIV = 1 |
Yes |
Yes |
Yes |
| ePWM |
ePWM: ESM Source for Trip Zone is not Supported |
Yes |
Yes |
Yes |
| ePWM |
ePWM: ePWM One-Shot/CBC Trip Event DCxEVTy.force Does Not Set
the Trip Condition |
Yes |
Yes |
Yes |
| ePWM |
ePWM: For ePWMs Using Global Load in One-Shot Load Mode, Global
Load of Registers may get Delayed When a Write to the
GLDCTL2.OSHTLD Register Occurs Within 3 TBCLKs of the Global
Load Event |
Yes |
Yes |
Yes |
| Flash |
Flash: Stand-alone CPU1/CPU3 Reset With Flash Prefetch Enabled
may Cause NMI to CPU1/CPU3 |
Yes |
Yes |
No |
| FOTA |
FOTA: Secure FOTA With Encryption does not Work |
Yes |
Yes |
No |
| HRPWM |
HRPWM: HRPWM High-Resolution Period Shadow to Active Loading
Occurs Every ZERO Event, Even if Shadow to Active Load for
Period is Set to Only Load on SYNC |
Yes |
Yes |
Yes |
| HSM |
HSM: HSM ROM Code Does Not Boot HSMRT Image of Size Greater
Than 191KB |
Yes |
Yes |
No |
| LIN |
LIN: LIN Unable to Wake Up Using 0xF0 Wake-Up
Key |
Yes |
Yes |
Yes |
| MCD |
MCD: Missing Clock Detect Should be Disabled When the PLL is
Enabled (PLLCLKEN = 1) |
Yes |
Yes |
Yes |
| MEMSS |
MEMSS: Data Line Buffer (DLB) for RAM Causes Data Coherency
Issue |
Yes |
Yes |
Yes |
| ROM |
ROM: By Default, GPIO4 is Configured as ERRORSTS by ROM Code
and Driven High |
Yes |
No |
No |
| SDFM |
SDFM: Dynamically Changing Threshold Settings (LLT, HLT),
Filter Type, or COSR Settings Will Trigger Spurious Comparator
Events |
Yes |
Yes |
Yes |
| SDFM |
SDFM: Dynamically Changing Data Filter Settings (Such as Filter
Type or DOSR) Will Trigger Spurious Data Acknowledge
Events |
Yes |
Yes |
Yes |
| SDFM |
SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields
CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock
Cycles can Corrupt SDFM State Machine, Resulting in Spurious
Comparator Events |
Yes |
Yes |
Yes |
| C29 CPU Subsystem |
C29 CPU Subsystem: DTHE Interrupts and DMA Events Not Triggered
in C29 CPU Subsystem for HS-FS Devices |
Yes |
Yes |
No |
| System |
System: Device Reset Remains Asserted When VDD Voltage Ramps
Before VDDIO |
Yes |
Yes |
Yes |
| System |
System: Pending Misaligned Reads in the Pipeline After CPU Goes
to Fault State Preventing NMI Vector Fetch |
Yes |
Yes |
No |
| UART |
UART: UART FIFO Gets Cleared on Continuous Debugger
Reads |
Yes |
Yes |
Yes |
| VSSOSC |
VSSOSC: Coupling From Adjacent Pins X1 or X2 may Prevent Proper
Boot |
Yes |
No |
No |