SWRA601N April 2019 – November 2025 CC1350 , CC1352P , CC1352P7 , CC1352R , CC2340R2 , CC2340R5 , CC2340R5-Q1 , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP , CC2674P10 , CC2674R10 , CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Question: What does the Declaration ID cost?
Answer: Details on declaration and listing fees can be found on the Bluetooth SIG Qualification & Listing Fees page.
Question: Can I reuse TI's Declaration ID when listing my product with Bluetooth SIG?
Answer: No. Each product must obtain a Declaration ID. Users can reference TI's qualified components or subsystems (QDID's) in the product's listing, as noted in Section 2, to reduce the amount of testing required to qualify the end product.
Question: If I do not put the Bluetooth logo on my product, do I still need to list my product with Bluetooth SIG?
Answer: For more information, see the Do I Need to List or Qualify My Product? guide on the Bluetooth SIG website. Additional questions on this topic needs to be directed to Bluetooth SIG directly by the contact information. Note that TI cannot determine whether a product must be listed or qualified as this is the customer's responsibility to adhere to all regulatory, certification and qualification requirements.
If users determine to list (certify) the product with BT SIG, then follow the process that is listed under Section 2.3. Users can combine with the TI BLE-Stack QDID (this saves the bulk of the testing). Test only the adopted services users are using with the PTS tool and do the RF-PHY testing (if users are not using a pre-certified module). The TI software has all the necessary hooks to enable the RF-PHY testing on the device side.
If users determine to not list the product with BT SIG, then these steps are not required. However, users need to perform regulatory testing (for example, FCC) depending on where to sell or ship the product.
Question: My test facility has said that the QDIDs are expired and, thus, ineligible for use, or I need to test with the latest TCRL.
Answer: The introduction of QDPRv3 removes the three-year expiration of QDIDs (now called DNs). TI recommends using the most recent QDID/DN during the qualification process. The QDIDs and DNs listed in this document are still valid and indicated as such when submitted to the SIG Qualification Listing Interface. There is no certification requirement to test with updated TCRLs when referencing a QDID/DN.
Question: What is a Bluetooth Qualification Consultant (BQC)?
Answer:
Question: I have created my own proprietary profiles, do I need to qualify them?
Answer: No, those are not part of the qualification process. However, note that the profiles need to follow the GATT protocol (that is, have a primary service, characteristic declarations with proper formatting, and so forth) and use 128-bit custom UUIDs.
Question: Can I reuse the CC2640 or CC254x FCC Certification?
Answer: The CC2640 and CC254x devices are wireless MCUs and thus cannot be individually certified by the FCC (or any regulatory body) since the wireless MCU + external RF design combination must be considered for regulatory listing purposes. However, users can reuse a module certification (MCU + Antenna) provided this is pre-certified with the respective regulatory body and users follow the layout placement guidelines from the data sheet. For example, the CC2650 Module from TI (CC2650MODA [12]) has FCC, ETSI, IC (Canada) and Japan regulatory pre-certification. A listing of modules that incorporate TI Bluetooth Low Energy wireless MCUs can be found on the main Bluetooth Low Energy Wiki page. TI provides the necessary interfaces to allow you to perform the required regulatory testing. For more details, see the following regulatory sections.
Question: Where can I find a list of test facilities to perform regulatory and Bluetooth testing?
Answer: A list of Test Facilities can be found on the Bluetooth SIG website (requires login). Many of these test facilities can also perform regulatory testing.
Question: My test lab is requesting me to fill out a form. Where can I find the required information?
Answer: All of the device-specific information can be found in the wireless MCU data sheet and the RF-PHY Test Parameters table listed above. The remaining items are obtained by performing actual measurements on the board using Direct Test Mode (DTM) or Modem Test Commands. Details about the internal radio architecture needed for regulatory filing can be obtained by reviewing TI CC254x and CC26xx FCC filings. For more information, see Section 3.