TIDUF68A February   2024  – March 2025

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
    1. 1.1 Key System Specifications
  8. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
    3. 2.3 Highlighted Products
      1. 2.3.1 LMG2100
      2. 2.3.2 INA241A
      3. 2.3.3 AMC0106M05
      4. 2.3.4 LMR38010
  9. 3System Design Theory
    1. 3.1 Three-Phase GaN Inverter Power Stage
      1. 3.1.1 LMG2100 GaN Half-Bridge Power Stage
    2. 3.2 Inline Shunt Precision Phase-Current Sensing
      1. 3.2.1 INA241A Ultra-Precise Current Sense Amplifier with Enhanced PWM Rejection
      2. 3.2.2 AMC0106M05 Precision, ±50mV Input, Functionally Isolated, Delta-Sigma Modulator
    3. 3.3 Phase Voltage and DC Input Voltage Sensing
    4. 3.4 Power-Stage PCB Temperature Monitor
    5. 3.5 Power Management
      1. 3.5.1 48V to 5V DC/DC Converter
      2. 3.5.2 5V to 3.3V Rail
    6. 3.6 Interface to Host MCU
  10. 4Hardware, Software, Testing Requirements, and Test Results
    1. 4.1 Hardware Requirements
      1. 4.1.1 TIDA-010936 PCB Overview
      2. 4.1.2 TIDA-010936 Jumper Settings
      3. 4.1.3 Interface to C2000™ MCU LaunchPad™ Development Kit
    2. 4.2 Software Requirements
    3. 4.3 Test Setup
    4. 4.4 Test Results
      1. 4.4.1 Power Management and System Power Up and Power Down
      2. 4.4.2 GaN Inverter Half-Bridge Module Switch Node Voltage
        1. 4.4.2.1 Switch Node Voltage Transient Response at 48V DC Bus
          1. 4.4.2.1.1 Output Current at ±1A
          2. 4.4.2.1.2 Output Current at ±10A
        2. 4.4.2.2 Impact of PWM Frequency to DC-Bus Voltage Ripple
        3. 4.4.2.3 Efficiency Measurements
        4. 4.4.2.4 Thermal Analysis
        5. 4.4.2.5 No Load Loss Test (COSS Losses)
      3. 4.4.3 Phase-Current Sensing
  11. 5Design and Documentation Support
    1. 5.1 Design Files [Required Topic]
      1. 5.1.1 Schematics
      2. 5.1.2 BOM
      3. 5.1.3 PCB Layout Recommendations
        1. 5.1.3.1 Layout Prints
      4. 5.1.4 Altium Project
      5. 5.1.5 Gerber Files
      6. 5.1.6 Assembly Drawings
    2. 5.2 Tools and Software
    3. 5.3 Documentation Support
    4. 5.4 Support Resources
    5. 5.5 Trademarks
  12. 6About the Author
  13. 7Recognition
  14. 8Revision History

Impact of PWM Frequency to DC-Bus Voltage Ripple

A key function of the bus capacitor is to smooth the bus voltage and provide transient current at the switching moment to keep the ripple of the bus voltage small enough.

When the PWM switching frequency is increased, the requirements for bus capacitance are reduced. Because the switching time of the FET becomes shorter, the amount of charge required by the capacitor becomes smaller, so using a higher PWM switching frequency can reduce the required bus capacitance value.

Usually, electrolytic capacitors are used as bus capacitors. Electrolytic capacitors can provide sufficient capacitance, but also have disadvantages, such as huge size, short life, poor high-frequency characteristics, and so forth. In comparison, ceramic capacitors are more stable and smaller, but the capacitance ceramic capacitors can provide is limited. The following test attempts to replace electrolytic capacitors with ceramic capacitors by increasing the PWM frequency.

Determine whether smaller ceramic capacitors can be used by testing the bus ripple of electrolytic capacitors and ceramic capacitors at different frequencies. This test used 60μF and 100μF ceramic capacitors (PN: C3225X7R2A106K250AC × 6 or 10) and 100μF electrolytic capacitor (PN: ECA2AM101).


TIDA-010936 DC-Link Voltage AC Ripple at 48VDC, 8kHz–80kHz PWM, PH_I = 5ARMS

Figure 4-18 DC-Link Voltage AC Ripple at 48VDC, 8kHz–80kHz PWM, PH_I = 5ARMS

As Figure 4-18 shows, as the frequency increases, the ripple on the bus gradually decreases, so capacitors with smaller capacitance can be used. But ceramic capacitors have significantly larger voltage ripple at low frequencies (< 80kHz). Because the actual capacitance of this 10μF ceramic capacitor is only 2.2μF at a voltage of 50V, the actual effective capacitances corresponding to the 60μF and 100μF ceramic capacitors in Figure 4-18 are 13.2μF and 22μF. Therefore, the ripple is larger than that of the 100μF electrolytic capacitor.

When the PWM frequency increases to 80kHz, the voltage ripple of a 100μF ceramic capacitor and an electrolytic capacitor is similar. Therefore, the ultra-low switching loss of GaN can be used to increase the PWM frequency to 80kHz. At the same time, the electrolytic capacitor can be replaced with a ceramic capacitor of the same capacity to achieve a smaller size.


TIDA-010936 Ceramic Capacitor Capacitance vs Voltage Curve

Figure 4-19 Ceramic Capacitor Capacitance vs Voltage Curve