TIDUFB3 July 2025
The TPS7H4010-SEP synchronous buck converter is selected to generate the required 1.2V directly from the 12V rail. TI's estimate is that the DDR_VDDQ rail for DDR4 requires up to 3A and the VLDOIN of the downstream TPS7H3302-SEP requires up to 3A; therefore, the full 6A capability of the TPS7H4010-SEP is used.
A switching frequency of 1MHz and a 0.8μH XAL5030-801ME_ inductor are selected to provide a reasonable balance of design size and efficiency. Additionally, the typical component selection table in the TPS7H4010-SEP data sheet is consulted to make sure the values are close to the recommended selection. This is confirmed through a load step and Bode plot measurement as shown in Section 4.3.2. A 50Ω resistor is placed in series with the top feedback resistor and an option for a feed-forward capacitor is implemented to enable easier measuring and optimization of the control loop.
Next, the output voltage ripple is determined. First the inductor ripple is calculated as shown in Equation 9. An inductor ripple current of 1.35A is calculated.
where
Next, two 100µF electrolytic capacitors and one 22µF ceramic capacitor is selected. Using the K-SIM tool from Kemet, the output impedance of these parallel capacitors at 1MHz is determined to be approximately 4.2mΩ. Multiplying the impedance by the inductor ripple current gives the approximated output ripple of ±5.7mV.
Finally, the output voltage is configured using a resistor divider connected to the feedback pin. An RFB_TOP of 50.55kΩ (50.5kΩ in series with a 50Ω) and RFB_BOT of 261kΩ are selected which results in a nominal output voltage of 1.201V. Using the data sheet feedback voltage parameter 0.987V minimum and 1.017V maximum along with 0.1% resistor tolerances (using a sum of squares to get ±0.14% error contribution), the overall DC accuracy can be approximated using Equation 10 and Equation 11. The accuracy is calculated to be –1.96% and +1.30%.
One additional consideration for accuracy is if auto mode is enabled. Auto mode results in higher efficiency at light loads at the expense of worse load regulation. Consulting the TPS7H4010-SEP load and line regulation image in the TPS7H4010-SEP data sheet and looking at the approximate 0.08V increase at light load for a 5V application, auto mode is approximated to add an additional error of +1.6%. Therefore, if auto mode is enabled, the accuracy is –1.96% and +2.90%. This error is acceptable for this rail, and therefore auto mode is enabled.
Table 3-4 shows a summary of these calculations.
| PARAMETER | DESCRIPTION OR TYPICAL VALUE |
|---|---|
| VIN | 12V |
| VOUT | 1.2V |
| IOUT(max) | 6A |
| fSW, switching frequency | 1MHz |
| DC Accuracy | –1.96%, +2.90% |
| Output ripple | 5.7mVpp |
| LSW, output inductor | 0.8µH, XAL5030-801ME_ |
| COUT, output capacitance | 2x100µF T520B, 1x22µF ceramic |
| CIN, input capacitance | 3x10µF ceramic, 1x470nF ceramic |
| tSS, soft start time | 6.3ms (SS float) |
| Bias connection | Connected to external 3V3_VCCO |
| Mode | Auto enabled |
Figure 3-9 1V2_MEM Schematic
Figure 3-10 1V2_MEM Layout