TIDUFE5 July 2025
The three-phase voltages, currents, and fluxes of AC motors can be analyzed in terms of complex space vectors. With regard to the currents, the space vector can be defined as follows:
where
Figure 3-6 shows the stator current complex space vector.
In Figure 3-6, (a, b, and c) are the three-phase system axes. This current space vector depicts the three-phase sinusoidal system. This still needs to be transformed into a two-time invariant coordinate system. This transformation can be split into two steps: