This reference design is implemented using a PCB with two layer, 1oz copper with a
single-side SMD component placement considering the cost sensitivity of the
application. There are several important aspects to remember while designing the
PCB. In the following list, system-level placement and layout of each block is
explained.
Components in the high-power path are kept on the outer edges of the PCB using the
minimum distance possible. The microcontroller is placed at the center considering
the optimum distance from all the power blocks that need to be controlled. Pin
assignment is set to minimize the control signal trace and feedback signal trace
distance and the crossing between analog and digital signals.
- AC Line Protection and EMI
Filter
- AC line protection components are closely placed
within the minimum distance of the connection path. Earth connection
guarding is provided around the protection and EMI filter circuit.
- An active EMI filter is placed at the optimum
distance so as to stay closer to switching and to have the minimum
distance to connect to the EARTH terminal.
- IPFC Drive
In IPFC drive, three current
paths are very critical for PCB layout - the high power AC loop, DC loop,
and gate drive loop. These paths need to be short with the maximum width
possible to reduce parasitic-loop inductance.
- AC loop – Consists of
diode bridge (source), inductor, and MOSFET drain and MOSFET source
(return). On this loop, especially the connection between the inductor,
the MOSFET Drain and Diode Anode handle high frequency and high power.
Special care is taken while connecting this node to minimize parasitic
inductance by reducing the distance and increasing the copper area.
- DC loop – Consists of
diode bridge (source), inductor, diode, capacitor, load (return). To
distribute the RMS current stress evenly, place the bank of electrolyte
capacitors such that the electrical distance of each one from the diode
cathodes remains approximately the same. This design uses a copper plane
for the VDC and PGND connection. To suppress the
high-frequency component, a metal-film capacitor is placed just next to
the cathode of the diode. The capacitor minimizes the loop inductance
significantly.
- Gate drive loop –
Consists of driver power supply (source), gate driver IC, MOSFET gate,
and MOSFET source pin (return). This design uses parallel arrangement
for two phases of IPFC to minimize the other two AC/DC loops. Because of
this parallel arrangement, the outer phase MOSFET gate is inaccessible
to the gate driver. An SMD insulated thick jumper is used to connect the
gate driver signal to MOSFET gate.
- Compressor and Fan Drive
- With the highest ripple requirement, a compressor
drive is placed closest to the DC bus capacitor bank of the IPFC drive
and a fan is placed next to the compressor.
- The low-side shunt resistor method with 4-wire
sensing is implemented for current sensing. A differential pair with
impedance matching resistors is used to connect the sensing signal from
the shunt resistors to the op-amp circuit. Shunt resistors are placed
near the module with an immediate ground copper plane connection.
- Auxiliary Power Supply
- With the lowest power and ripple requirement,
auxiliary power is placed after the fan drive. A dedicated copper plane
is used to connect the APS ground to the DC bus capacitor bank. This
arrangement minimizes interference between the high frequency and high
power motor current and control circuit.