Permanent Magnet Synchronous motor (PMSM) has a wound stator, a permanent magnet rotor assembly and internal or external devices to sense rotor position. The sensing devices provide position feedback for adjusting frequency and amplitude of stator voltage reference properly to maintain rotation of the magnet assembly. The combination of an inner permanent magnet rotor and outer windings offers the advantages of low rotor inertia, efficient heat dissipation, and reduction of the motor size.
- Synchronous motor construction: Permanent magnets
are rigidly fixed to the rotating axis to create a
constant rotor flux. This rotor flux typically has
a constant magnitude. The stator windings, when
energized, create a rotating electromagnetic
field. To control the rotating magnetic field,
this is necessary to control the stator
currents.
- The actual structure of the rotor varies
depending on the power range and rated speed of
the machine. Permanent magnets are designed for
synchronous machines ranging up-to a few
kilowatts. For higher power ratings, the rotor
typically consists of windings in which a DC
current circulates. The mechanical structure of
the rotor is designed for the number of poles
desired, and the desired flux gradients
desired.
- The interaction between the stator and rotor
fluxes produces a torque. Since the stator is
firmly mounted to the frame, and the rotor is free
to rotate, the rotor can rotate, producing a
useful mechanical output as shown in Figure 3-4.
- The angle between the rotor magnetic field and
stator field must be carefully controlled to
produce maximum torque and achieve high
electromechanical conversion efficiency. For this
purpose a fine tuning is needed after closing the
speed loop using a sensorless algorithm to draw
the minimum amount of current under the same speed
and torque conditions.
- The rotating stator field must rotate at the same
frequency as the rotor permanent magnetic field;
otherwise, the rotor can experience rapidly
alternating positive and negative torque. This can
result in less-than-designed-for torque
production, and excessive mechanical vibration,
noise, and mechanical stresses on the machine
parts. In addition, if the rotor inertia prevents
the rotor from being able to respond to these
oscillations, the rotor can stop rotating at the
synchronous frequency, and respond to the average
torque as seen by the stationary rotor: Zero. This
means that the machine experiences a phenomenon
known as pull-out. This is also the reason
why the synchronous machine is not self
starting.
- The angle between the rotor field and the stator
field must be equal to 90ยบ to obtain the highest
mutual torque production. This synchronization
requires knowing the rotor position to generate
the right stator field.
- The stator magnetic field can be made to have any
direction and magnitude by combining the contribution of different stator phases
to produce the resulting stator flux.