SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
In summary, the DSP_INTC accepts up to 124 event inputs, and flexibly maps those down to 12 interrupt inputs to the DSP. The mapping can be 1:1 (input:output), or can use the event combiner to map multiple interrupts (within a 32-bit group) to one of the DSP interrupt inputs. In general, many of the 124 interrupt controller inputs are collected within the DSP C66x CorePac, and are NOT available at the DSP C66x CorePac boundaries.
The C66x CPU dropped event is exported outside the C66x CorePac in DSP subsystem, and can be enabled to trigger the ERRINT_IRQ aggregated interrupt output. See also corresponding "INTERR" event listed in the Table 5-5.
The dropped CPU event is not exported outside DSP subsystem. However it is merged (OR-ed) along with other error event sources within the DSP subsystem to produce a single ERRINT_IRQ interrupt exported outside the DSP subsystem.
For more details on ERRINT_IRQ generation and asscoiated event registers at DSP_SYSTEM level, refer to the Section 5.3.4.2.2.
Part of the input interrupts, generated by DSP peripherals that are located outside the DSP C66x CorePac - DSP_EDMA (DSP_EDMA_CC, DSP_EDMA_TC0, DSP_EDMA_TC1) , DSP_MMU0, DSP_MMU1 and DSP_NoC, are also mapped to outputs at the DSP subsystem boundary, such that they can be exported to system hosts (MPU, and so forth) via the device IRQ_CROSSBAR.
Of particular interest, MMUs (DSP_MMU0 and DSP_MMU1) interrupts will typically be serviced by the device MPU instead of by the local DSP core.
Any interrupt input at DSP subsystem boundaries (i.e. excluding the DSP subsystem internal IRQ sources that reside in and outside the DSP C66x CorePac) can be used to wake-up the DSP subsystem from an IDLE state. This is described in the Section 5.3.3.4.3 and is controlled by the DSP_SYSTEM logic register DSP_SYS_SYSCONFIG [3:2] IDLEMODE bitfield along with the DSP_SYS_IRQWAKEEN0 / DSP_SYS_IRQWAKEEN1 registers.
The DSP_SYS_IRQWAKEEN0 / DSP_SYS_IRQWAKEEN1 bits MUST be enabled for externally mapped interrupts (DSP_INTC[95:32]) to be serviced by the DSP regardless of the DSP power state (IDLE or non-IDLE).
The DSP C66x CorePac DSP_INTC registers are NOT readable by any entity other than the C66x CPU, because they are part of the DSP_ICFG C66x CorePac internal configuration space (see also the Section 5.3.10). Hereby, only the C66x itself is able to service these interrupt events. The only way for these interrupts to be cleared is for the DSP CPU to clear the state in the EVTFLAGi (where i=0 to 3) register, or via reset assertion.
For cases where the DSP maps an interrupt directly, the DSP is not strictly required to clear the EVTFLAGi register. User software must take the extra step of clearing the EVTFLAGi to cause the corresponding output interrupt to be cleared and re-asserted upon a new input event assertion.