SPRUHZ7K August 2015 – April 2024 AM5706 , AM5708 , AM5716 , AM5718 , AM5718-HIREL
In the case of a multiplexed data stream input the channels that should be used are VIP(X)_MULT_PORT(Y)_SRC(Z). Where X is the specific VIP slice of the instance that wants to be used and port Y is the port A or port B that is receiving the data. Finally Z is the channel number. For Split line mux mode the LSB of the channel will determine, if the line is a split line or a complete line. This is required so that the data streams do not get mixed when a channel ends without completing a line. In this mode the data will always be sent out as 422 Interleaved data to the destination specified in the descriptor.