SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
For compatibility with existing TI parts, the packet format given in Figure 26-9 can be used in most cases. This packet format is supported through the use of the commands CMD_PROP_TX and CMD_PROP_RX.
Figure 26-9 Standard Packet FormatA more flexible packet format is also possible, as defined in Figure 26-10. This format is supported by the commands CMD_PROP_RX_ADV and CMD_PROP_TX_ADV. The format in Figure 26-9 is an example of this format.
Figure 26-10 Advanced Packet Format