SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Some instructions with an 8-bit or 10-bit immediate value may be extended to a 16-bit immediate value by executing a prefix instruction,
pfix
, immediately before it. The prefix is valid for the next instruction only.
The last column in the following tables indicates which immediate value may be extended, if any.
The Sensor Controller Studio assembler adds prefix instructions automatically as needed, and detects immediate values that are invalid or out of range. The assembler also repairs branch instructions where the target address is out of range.