SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Table 16-1 lists the key power management features.
| Key Features | Description |
|---|---|
| Auto-power management | The SimpleLink device has advanced internal power-management logic that puts it in LPDS (low-power deep sleep) in a manner transparent to the host. |
| 802.11 Power save | Use of the power-save feature of the 802.11 standard allows the device to consume low power while maintaining a connection to an access point. |
| IoT Low Power (CC313x and CC323x only) | The SimpleLink Wi-Fi device supports the new WFA low power mode during connection. In this mode, the device negotiates (during the connection) the maximum sleep interval allowed. Based on the value and its own configuration, the device can extend the sleep interval. |
| Power-optimized out of the box | Device is power-optimized by default. No configuration by the host is necessary to activate these features. |
| Fast connect | Can connect to the last known network without performing a WLAN scan, which dramatically decreases connection time and saves power. |