SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Open a serial connection application like TeraTerm or Putty (any other terminal emulator program can be used), and configure the settings:
| Parameter | Value |
|---|---|
| Baud Rate | 921600 |
| Data Bits | 8 |
| Stop Bits | 1 |
| Parity | None |
| Flow Control | None |
If you are using a CC31XXEMUBOOST, connect the fourth port in Device Manager.
Configure the terminal emulation to work in binary mode (and not textual/ASCII mode) and record the log. Here are some examples:
Tera Term
Setup → Serial Port…
Figure 20-1 Tera Term Port SettingsFile → Log...
Figure 20-2 Tera Term Log SettingsPutty
On the left side of the screen, select Connection → Serial:
Figure 20-3 Putty Port SettingsIn the menu screen before connecting to the port:
Figure 20-4 Putty Log Settings