SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Once a profile is configured, the device tries to connect to that profile to confirm that it was properly provided (the user might type the wrong SSID or password), and that the wireless network is valid. If the connection attempt was successful (such as a WLAN connection was established and an IP address was acquired), the device tries to provide the end-user who configured the profile a feedback (through a message on their tablet or smartphone app) indicating a successful connection.
If the feedback about a successful connection was received by the user, the profile is confirmed and the provisioning process ends.
If the connection was not successful, or if the connection was successful but the feedback was not delivered to the user, the confirmation fails, and the device waits for the user to try to configure another profile, as shown in Figure 17-1.
Figure 16-1 The Provisioning Environment