SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When the device is in AP mode, posts to /api/1/wlan/en_ap_scan/station_action can be performed to disconnect stations from the device. The station to disconnect is given by the parameters in Table 10-11.
| Name (code) | Description | Example |
|---|---|---|
| Station number to disconnect (__SL_P_CRR) | The number of the station to disconnect. Must be from 1 to the maximum number of station as set by the user. | __SL_P_CRR=1 |
For example, the following request disconnects station 1:
POST /api/1/wlan/en_ap_scan/station_action HTTP/1.1
Host: mysimplelink.net
Content-Type: application/x-www-form-urlencoded
__SL_P_CRR=1