SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Table 10-18 lists the connection policies status tokens.
| Token | Name | Value and Usage |
|---|---|---|
| __SL_G_P.E | Auto Connect | If auto connect is enabled, returns Checked, else returns Not_Checked. Used in the auto connect checkbox. |
| __SL_G_P.F | Fast Connect | If fast connect is enabled, returns Checked, else returns Not_Checked. Used in the fast connect checkbox. |
| __SL_G_P.G | Any P2P | If any P2P is enabled, returns Checked, else returns Not_Checked. Used in the Any P2P checkbox. |
| __SL_G_P.P | Auto Smart Config | If auto smart config is enabled, returns Checked, else returns Not_Checked. Used in the Auto Smart Config checkbox. |