SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
User pages are any content stored under the /www/ or /www/safe/ path on the file system. The content can be set by the application, either as part of the programming process or using the host application file system API.
The previously mentioned paths are used only to organize files on the file system, and must not be part of a URL when linking to resources. For example, the URL of a file named example.html that is placed at /www/user_directory/example.html is http://deviceIP/user_directory/example.html.
Placing any file under the /www/ path of the file system makes it a resource which the HTTP server can serve to its clients. These resources are static, as their content remains constant. Serving these resources is handled completely by the HTTP server and is transparent to the host as seen in Figure 10-4.
Figure 9-4 Static Pages