The open-create or open-create-write creates a new file, and as part of the function the device allocates the storage for the file. The size of the allocated storage is determined by the maximum size parameter. The close function makes the opened file valid.
A file created but not closed has allocated storage (according its maximum size), but does not have a valid copy.
Because the process of creating a file involves updating the file allocation table on the SFLASH, TI recommends minimizing the creation of files. If it is required to update the file content, open the file for write rather than delete and recreate it.
For a secure file, the default behavior of the
file creation function is to generate the file tokens (including the master): the
master token is returned as the function output, and all other tokens can be
retrieved using the sl_FsGetInfo() function. Further information regarding the file
tokens can be found in the CC3x20, CC3x35, and CC3x30 SimpleLink™ Wi-Fi® Internet-on-a
chip™ Solution Built-In Security Application Report.
The sl_FsOpen() function tests that the file storage can be allocated, that the file does not exist, and that the creation flags are valid. The smallest memory hole that fits the requested size is allocated (as fragmentation is not supported). If an error occurs while attempting to open a file, the function returns a negative value which represents the error number; Table 9-3 shows a partial list of errors that might be returned by the creation function.
Table 8-3 Creation Function Errors| Error | Description |
|---|
| SL_ERROR_FS_NOT_ENOUGH_STORAGE_SPACE | No available storage for the file. |
| SL_ERROR_FS_FILE_ALREADY_EXISTS | File with the same name already exists. |
| SL_ERROR_FS_NO_AVAILABLE_NV_INDEX | Number of opened files exceeded. |
| SL_ERROR_FS_FILE_INVALID_FILE_SIZE | The maximum file size is set to 0. |
The create file input parameters are:
- Filename: The filename is a string of up to 180 bytes; TI recommends using short filenames (explained in Section 9.3); the file name is not case-sensitive.
- Maximum file size
- When creating a file, the storage for the file is allocated according the requested maximum file size. For an existing file, the maximum file size cannot be changed; thus, when defining the maximum size of a file, the future growth of the file should be considered.
- Creating a file with the FAILSAFE flag creates the file with a copy, thus the allocated storage size for the file is doubled.
- Because the smallest erase unit of a SFLASH is 4096 bytes, the file system allocates storage size, which is aligned to 4096 bytes.
- File tokens: The token is the key for accessing a secure file; for a nonsecure file, it is set to zero. The file creation function returns the file token. By default, the device generates the file master token and returns it to the host. The default behavior of the token creation can be overridden by special creation flags.
- Creation flags: The creation flags are set during the file creation and cannot be changed afterward. The following is a list of creation flags:
- SL_FS_CREATE_FAILSAFE: A file opened with failsafe has double copies, but only one copy is considered to be active at a time. Each time the file is opened for write, the file storage is erased. If the system is powered off while writing a file with no failsafe, the file content is lost. If the system is powered off while writing a file with failsafe, the old content becomes the active one. Using the FAILSAFE doubles the file allocated storage. If the bundle feature (used for OTA) is used with the file, this flag is mandatory.
- SL_FS_CREATE_SECURE: A file created as secure has its content encrypted on the SFLASH. Access to the file is limited, and requires a file token. See the security application notes file for more information about secure files.
- SL_FS_CREATE_NOSIGNATURE: The flag is relevant only for secure files. By default, a secure file has a signature, which authenticates the file creator. See the security application notes for more information about how to create file signature.
- SL_FS_CREATE_STATIC_TOKEN: Relevant only for secure files. This flag changes the default behavior of the file tokens creation: with this flag, the file tokens are not changed each time a file is opened for write.
- SL_FS_CREATE_VENDOR_TOKEN: Relevant only for secure files. This flag changes the default behavior of the file tokens creation: with this flag, the file master tokens are set by the host.
- SL_FS_CREATE_PUBLIC_WRITE: Relevant only for secure files. This flag changes the default behavior of the file tokens creation: with this flag, the file can be written without a token, but for a read operation a token is required.
- SL_FS_CREATE_PUBLIC_READ: Relevant only for secure files. This flag changes the default behavior of the file tokens creation; with this flag, the file can be read without a token, but for a write operation a token is required.
- Flags: The following flags are not creation flags, but can be set when creating or opening an existing file for write.
- SL_FS_WRITE_BUNDLE_FILE: Used for the bundle commit feature; for new files, the FAILSAFE flag is not a precondition for this flag.
- SL_FS_WRITE_ENCRYPTED: Used for secure content download.
If the application creates a file once, it can then be created by the Image Creator tool with the default content. The application can then update the file when required.