SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
Device Tokens are special text strings inside a resource, which the HTTP server substitutes with values just before serving the resource to the requesting client (see Section 10.5 for details). These tokens are updated by the SimpleLink device every time a resource is served, which lets users create pages with some dynamic content (various parameters of the SimpleLink device) without any involvement from the host, as shown in Figure 10-5.
Figure 9-5 Custom Pages With Device Tokens