SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The required size for the programming image can be observed in the UniFlash Image Creator log. The Image Creator tool maintains a log which is displayed during the image creation; the log displays how many blocks are allocated for each file, and an estimation of the total required storage size.
After the SFLASH is programmed, the file list function (host driver) retrieves information about the existing files and the number of allocated blocks per file.
The get storage info function contains information about the device usage, information about the device capacity, the largest available gap, and so forth.
Figure 9-1 is an example of the Image Creator log, which is displayed during the image generation.
Figure 8-1 Image Creator Log