SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
When provisioning is started in AP + SC + external configuration mode, the host can start sending commands to the networking subsystem only after the external configuration ready event is received. When the host identifies that a user has started a provisioning process using the external configuration method, it should order the networking subsystem to stop the internal provisioning process. When the internal provisioning process is stopped, the host can continue with its external provisioning process.
Figure 16-8 External Configuration Method: WAC