SBASAE4 December 2025 ADS125P08
PRODUCTION DATA
The read register command is used to read register data. The command follows a two-frame protocol in which the read command is sent in one frame and the ADC responds with register data in the next frame. The first byte of the command is the base command value (40h) added to the 6-bit register address. The value of the second command byte is arbitrary, but is used together with the first byte for the CRC. The device outputs 00h as the register data for a read from an register outside the valid address range. The register data format is most-significant-bit first.
Figure 7-47 shows an example of reading register data using the 24-bit output frame size. Frame 1 is the command frame and frame 2 is the data response frame. The frames are delimited by taking CS high. The data response frame returns the requested register data byte, followed by the register address indication byte, and a 00h padded byte to complete the 24-bit frame. The 6-bit register address is right-aligned within the register address indication byte (padded with 00b at the MSB position). If desired, the data response frame can be shortened after the data byte by taking CS high.
Reading from a register address outside the valid address range returns the address FFh in the register address indication byte to indicate an error.
When reading multiple registers, full-duplex operation can be used to double the throughput of the read register operations by inputting the next read register command during the data response frame of the previous register.
Figure 7-48 shows an example of the read register operation using the 48-bit frame size in full-duplex operation. In frame 1, conversion data are output at the same time as the read register command is input (if the previous frame is not a read register command). The input command is padded with three don't care bytes to match the length of the output data frame. The padded input bytes are excluded from the CRC-IN code calculation. Frame 2 shows the input of the next command concurrent with the output of the previous register data. The CRC-OUT code includes all preceding bytes within the data output frame. The SPI_CRC_FAULTn bit of the STATUS_LSB header indicates if an SPI CRC error occurred and whether the read register command is accepted.