SBASAE4 December 2025 ADS125P08
PRODUCTION DATA
The circuit implementation in Figure 8-4 uses the analog supply to excite the bridge sensor. Use the bridge excitation voltage as the external reference voltage for the ADC to implement a ratiometric bridge measurement. Equation 32 through Equation 34 show how to derive the relationship between ADC output codes and the applied bridge signal using a pressure sensor as an example. Equation 34 shows that the output codes are independent of the excitation voltage in this ratiometric circuit implementation.
Where:
The guideline for selection of n is:
The example in Figure 8-4 shows a thermistor to measure the bridge temperature. The reference voltage output is used in this case to implement a ratiometric thermistor measurement. The conversion result according to Equation 36 is only dependent on the bias resistor (RBIAS) and the thermistor resistance (which strongly depends on the temperature).
Where n follows the guidelines of Equation 34.
Use one of the GPIO outputs to control a switch placed between the bridge sensor and GND for applications where the bridge sensor needs to be powered down periodically to save power.
For more information about resistive bridge sensor measurement circuits and the implementation using TI ADCs see the A Basic Guide to Bridge Measurements application note.