SBASAE4 December 2025 ADS125P08
PRODUCTION DATA
Set the FIFO_EN bit in the FIFO_CFG register to enable the FIFO buffer. As long as FIFO_EN is 0b, the FIFO buffer is not storing conversion results. In this case, only the last completed conversion result is available for read using the conversion data read operation as described in the Read Conversion Data section. Alternatively, use the continuous read mode as described in the Continuous Read Mode section.
When resetting the FIFO_EN bit to 0b, the FIFO is disabled and flushed. This clears all FIFO data, and resets the read pointer and write pointer.