SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The schematic in Figure 2-5 shows the startup circuit of the HART transmitter. When power is applied, voltage pulls up on LOOP+ to start up the TLV431B LDO to power the board.
The 249kΩ resistor allows current to flow through the 3.6V Zener diode, the voltage pulls up on the base of Q1. The Zener voltage starts the current through Q1 to turn on the LDO. The TLV431B LDO sets up the 3.3V supply.
As the 3.3V supply comes up, the control circuitry pulls current from Q3. This turns on Q2, which then takes over supplying current to the LDO.
When the 3.3V LDO output reaches the final value, the voltage at the emitter of Q1 rises. With the 3.6V driving the base of Q1 and 3.3V at the emitter, this voltage difference reduces the base-emitter voltage of Q1 to 0.3V. With a low base emitter voltage, Q1 shuts off. Q2 the maintains the current needed to drive LDO output and shunt the extra loop current. Because Q2 is the primary path of current through the transmitter, the transistor must be a PNP capable of high-power dissipation.
Take care when selecting the Zener diode. The voltage across the Zener diode varies with the loop voltage and the temperature of the circuit. This variance can change the VBE across Q1 and change the total current going through the start-up circuit. If the voltage is too high, the Zener diode sets Q1 to continue to source current after the circuit starts up. If the voltage is too low, the Zener diode prevents the TLVH431B from turning on. Verify proper start up by checking that the 3.3V supply starts up, and that Q1 turns off when in operation