SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The last of the physical layer tests are the carrier detect tests. During these tests, the modem is replaced with the HCF_TOOL-35 physical layer test interface. This tool is a HART modem interface with an adjustable output that can vary the amplitude of the tester HART signals. Figure 3-20 shows the HART carrier detect test setup.
The carrier detect tests verify what minimum amplitude of transmission is needed to identify the signal as a HART signal. The test also identifies the maximum in-band signal that is not identified as a HART signal. An oscilloscope is used to verify the amplitude of the signal. The test also verifies the time required for a start and stop with a HART minimum amplitude transmission.
For the carrier detect tests, the signal level is dropped from the typical 500mVPP level to 120mVPP. The HART modem communication must still be received by the transmitter. After completion, the signal level is dropped even further to 80mVPP, where the transmitter must reject any commands. Finally, the signal level is raised back to 120mVPP. The device must again receive HART communication from the test system. Each of these tests are performed while sending 100 HART commands to the transmitter.
After these tests are completed the start and stop time are re-tested with the 120mVPP signal to verify transmission. Table 3-8 reports the results for the Carrier Detect tests
| TEST | SIGNALING AMPLITUDE | MEASUREMENT | MAXIMUM | RESULT |
|---|---|---|---|---|
| Successful error-free communications | 120mVPP | 100 communication attempts | 0 errors | Pass |
| Unsuccessful Communications | 80mVPP | 100 communication attempts | 0 successful communications | Pass |
| Successful error-free communications (return) | 120mVPP | 100 communication attempts | 0 errors | Pass |
This test uses a 250Ω current sense resistor. Carrier start and stop times must be less than 5ms (less than 6 bit times).