SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The last of the HART tests verify that common-practice commands of the application layer (CAL) are implemented in the transmitter. The CAL test specification is described by HCF_TEST_4. These tests check for highly-recommended commands that are implemented in many HART devices. Here is a basic list of common-practice commands that can be implemented in HART devices and tested as part of the CAL tests:
Table 3-11 shows the set of common-practice command tests run by the HART tester. While the transmitter designed in this application note uses a HART stack that shows functionality of the device, this design is not a full-functioned device used as a real transmitter in an application. Many commands have been implemented, but not all are supported from this list of tests. This complete set of CAL tests take about 4 hours to complete.
| TEST NUMBER | DESCRIPTION | RESULT |
|---|---|---|
| CAL000 | Checks for common practice commands | Pass |
| CAL001 | Write protect test | Not implemented |
| CAL033 | Read device variables | Pass |
| CAL034 | Write primary variable damping value | Pass |
| CAL035 | Write primary variable range values | Pass |
| Primary variable units code unaffected by command 35 | Pass | |
| CAL036 | Set primary variable upper range value | Not applicable |
| CAL037 | Set primary variable lower range value | Not applicable |
| CAL040 | Enter/exit fixed current mode | Pass |
| CAL041 | Perform self test | Pass |
| CAL042 | Perform device reset | Pass |
| CAL043 | Set primary variable zero | Not applicable |
| CAL044 | Write primary variable units | Pass |
| CAL045 | Trim loop current zero | Pass |
| CAL046 | Trim loop current gain | Pass |
| CAL047 | Write primary variable transfer function | Not applicable |
| CAL049 | Write primary variable transducer serial number | Not applicable |
| CAL050 | Read dynamic variable assignments | Not applicable |
| CAL051 | Write dynamic variable assignments | Not applicable |
| CAL052 | Set device variable zero | Not applicable |
| CAL053 | Write device variable units | Not applicable |
| CAL054 | Read device variable information | Pass |
| CAL055 | Write device variable damping value | Not applicable |
| CAL056 | Write device variable transducer serial number | Not applicable |
| CAL060 | Read analog channel and percent of range | Not applicable |
| CAL062 | Read analog channels | Not applicable |
| CAL063 | Read analog channel information | Not applicable |
| CAL064 | Write analog channel additional damping value | Not applicable |
| CAL065 | Write analog channel range values | Not applicable |
| CAL066 | Enter/exit fixed analog channel mode | Not applicable |
| CAL067 | Trim analog channel zero | Not applicable |
| CAL068 | Trim analog channel gain | Not applicable |
| CAL069 | Write analog channel transfer function | Not applicable |
| CAL070 | Read analog channel endpoint values | Not applicable |
| CAL071 | Lock device | Not applicable |
| CAL072 | Squawk | Pass |
| CAL073 | Find device | Not applicable |
| CAL074 | Verify I/O system commands | Not applicable |
| CAL078 | Command aggregation | Not applicable |
| CAL079 | Write device variable | Not applicable |
| CAL080 | Verify device variable trim commands | Not applicable |
| CAL091 | Trending | Not applicable |
| CAL101 | Subsystem burst mode | Not applicable |
| CAL103 | Support for multiple burst messages | Pass |
| CAL104 | Smart data publishing | Pass |
| CAL107 | Write burst device variables | Pass |
| CAL108 | Write burst mode command number | Pass |
| CAL109 | Burst mode control | Pass |
| CAL115 | Event notification | Not applicable |
| CAL512 | Country code | Not applicable |
| CAL518 | Location description | Not applicable |
| CAL520 | Process unit tag | Not applicable |
| CAL523 | Read condensed status mapping array | Not applicable |
| CAL524 | Manipulating condensed status map | Not applicable |
| CAL526 | Status simulation | Not applicable |
As with the DLL and UAL tests, running the CAL tests from hartmenu generates a set of logs for the registration submission.