SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The next test is the carrier start and stop transient measurements. The test setup in Figure 3-11 is similar to the previous test where the carrier start and stop are measured. In this test setup, an HCF_TOOL-32 filter is measured by another channel of the oscilloscope. This low-pass filter removes the higher-frequency HART signal band and passes any signal below 25Hz. The filtered signal shows the current measurement of the primary variable. This test verifies that the HART transmission start and stop does not create any noise that interferes with the primary variable measurement.
Figure 3-11 shows the oscilloscope plots of the HART signal while being enabled and disabled. Additionally, the oscilloscope measures the same signal filtered through the HCF_TOOL-32. The HCF_TOOL-32 is capacitively coupled to the resistive load. The low-pass filtered signal in blue shows the output noise amplitude of the transmitter. Here, the specification requires a peak amplitude of 100mV maximum. The transmitter maximum shows a 22.1mVP-P noise amplitude for the transition noise. Table 3-3 reports the results of the scope measurements.
| TEST | MEASUREMENT | MAXIMUM | RESULT |
|---|---|---|---|
| Carrier start peak analog filter output | 21.8mVPP | 100mVPP | Pass |
| Carrier stop peak analog filter output | 22.1mVPP | 100mVPP | Pass |