SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Figure 2-3 shows the AFE881H1 HART detailed schematic transmitter design. The figure shows the loop power connection on the right side of the figure. Input protection is placed between the input terminals and the transmitter circuit. The positive loop connection then goes to a startup circuit for the board and powers an LDO. This LDO powers the AFE device, op-amps, and V-to-I control.
The LDO also drives a flyback converter acting as a boost to drive power across an isolation barrier. A set of digital isolators send communication across the isolation barrier. On the opposite side of the isolation is another LDO that powers the microprocessor.
The AFE881H1 controls the loop current through the V-to-I section. The DAC voltage sets the output from 0.3V to 2.5V. The output is sent through a V-to-I converter block using an OPA333 and an NPN bipolar junction transistor (BJT) that controls the loop current. In the constructed circuit, a MSP430FR5969 is used as the microprocessor, but is not shown in the figure.