SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Starting with the original diagram for the 4-20mA loop in Figure 1-1, HART can be added to the transmitter and receiver. HART communication uses the original 4-20mA loop and adds a two-way digital signal to the loop using HART modems. Again, this backwards compatibility makes HART any easy add-on to existing infrastructure. Figure 1-2 shows how HART is added to the basic 4-20mA loop.
The HART FSK is added to the signal controlling the current in the loop. In the transmitter, the HART modem receives the signal from the loop. The modem capacitively couples the input voltage to receive the HART signal. The modem also modulates the current to send the HART signal. This transmitted signal is superimposed onto the current representing the primary variable as measured by the sensor.
At the same time, the receiver measures the voltage across the resistor to measure the primary variable. In the HART-enabled receiver, a HART modem is used to both transmit commands and receive HART communication from the transmitter. However, the primary variable measurement requires a low pass filter to filter out the HART signal. A resistor is used to measure the current in the loop which represents the primary variable. The minimum resistance for HART communication is 230Ω, and 250Ω is often used.