The following simulation results
evaluate the impact of anti-pad size on return loss and impedance continuity in the design
example:
- Figure 3-2: Simulation model for landing pad and anti-pad structure.
- Figure 3-3: Return loss (S11) simulation result with different anti-pad size.
- Figure 3-4: TDR impedance simulation result with different anti-pad size.
Key observations:
- Without anti-pad (red curve), the impedance deviation is
maximized and the return loss (S11) is significantly degraded.
- Different anti-pad size results in different impedance change
and return loss (S11) performance.
- In this design example, an anti-pad
size 1.4 × wider than the landing pad achieves the best return loss (S11)
performance.
Key recommendations for AC coupling capacitor landing pad:
- Use anti-pad under the components when the landing pad size is larger than the matched
50Ω high-speed trace width (for example, IC pins, AC coupling capacitors, ESD diodes, line
fault resisters).
- The size of the anti-pad depends on the specific PCB stackup, the recommendation is to
perform a high-speed simulation to determine the proper anti-pad size.
- If possible, select a PCB stackup where the high-speed trace width matches the largest
component pad size (for example, 0402 pad size). This approach helps to eliminate the need
of anti-pads under the components and has the best impedance continuity.